Default memory usage
An empty project uses zero code memory and the
Used
memory parameter indicates 0 for memory consumption and steps in an empty project. A Micro800
controller contains a certain amount of memory and steps because the data portion contains:- System variables
- I/Os
- Reserved memory for temporary variables
- Reserved memory for user variables added during online changes
Controller | Memory Consumption | Step |
|---|---|---|
Micro810 | 5 KB | 456 |
Micro820 20 points | 14 KB | 591 |
Micro850 24 points | 15 KB | 657 |
Micro850 48 points | 15 KB | 659 |
Micro870 24 points | 15 KB | 657 |
Provide Feedback