View the controller mode
When connected to a
Micro800
controller, use Connection
to view the controller mode.Prerequisites
- The controller is online.
To view the controller mode
- InConnection, select
to expand the controller information. Available controller modes are as follows:- Program: The controller is in the non-running mode and can be programmed. The mode cannot be changed remotely.
- Remote program: The controller is in the non-running mode and can be programmed. The mode can be changed remotely.
- Run: The controller is in the running mode. The mode cannot be changed remotely.
- Remote run: The controller is in the remote running mode, displaying the connected values from the controller inFactoryTalk Design Workbench. The mode can be changed remotely.
Provide Feedback