View the controller fault status
When connected to the
Micro800
controller, use Connection
to view the controller fault status.Prerequisites
- The controller is online.
To view the controller fault status
- (optional) IfConnectionis hidden, open it by doing one of the following:
- From theViewmenu, selectConnection.
- Select
to open the Online center.
- InConnection, beside the controller name and catalog number, check the color of the toggle. If a fault occurs, the toggle turns red with an error icon.
Provide Feedback