Set up the connection path
Use
Online center
to set up the connection path for the controller by entering its IP address.To set up the connection path
- Select
to open Online center. - InOnline center, in thePathbox, enter the IP address of the controller.
- SelectEnter.
To clear the connection path, double-click the
Path
box, delete the IP address, and then select Enter
.Provide Feedback