Configurations on the controller diagnostics page
Configuration | Description |
|---|---|
Controller Identity | Displays the catalog number, firmware revision, series, serial number, and firmware boot code of the controller. |
Startup | |
Mode Behavior | Controls how the controller behaves during power-up. |
Fault Override | Displays the clear fault option during power-up. |
Memory Module or Memory Card | |
Load on power up | Determines if the controller restores the project from the memory module at power-up. The setting is selected in the memory module at power-up. |
Overwrite Ethernet settings | Determines if the current Ethernet settings will be overwritten by the settings in the memory module when restoring from the memory module. This setting only resides in the controller project and is not part of the memory module settings. Unlike load-always project settings that are backed up to and then read at power-up from the memory card, Overwrite Ethernet settings are read at power-up from the project setting residing in the controller and cannot be read directly from the memory card. |
Include variable values upon backup or restore | Determines whether to include the controller values when backing up or restoring the controller project. |
Catalog ID | Displays the model number of the controller or memory module. |
Project version | Displays the version of the project in the controller or memory module. |
Controller Information | |
CPU up time | Displays the total duration that the CPU has been active since its most recent power-up. |
Communication utilization | Displays the communication buffer space utilization rate of the current system. |
Summary | Displays:
|
Provide Feedback