DeviceNet scanner status codes
The 2080-DNET20 plug-in module adds DeviceNet capability to an L20E, L50E, or L70E controller.
Status value | Description |
|---|---|
65 | Autoscan Active (Scanner Only Status) |
67 | Reserved |
68 | Reserved |
69 | Reserved |
70 | Scanner failed DUP MAC check |
71 | Illegal value in Scan List |
72 | Device stopped communicating |
73 | Device does not match Scan List |
74 | Scanner has detected data overrun |
75 | No network traffic detected |
76 | No network traffic detected for scanner |
77 | Data size returned not math Scan List |
78 | Device in Scan List not active on subnet |
79 | Scanner failed to transmit a message |
80 | Scanner is in idle mode operation |
81 | Scanner is in fault mode operation |
82 | I/O fragment out-of-sequence |
83 | Device refused to be initialized |
84 | Device not yet initialized |
85 | Data size incorrect on a connection with this device |
86 | Device (slave) went into idle |
87 | Shared master has not allocated slave |
88 | Shared master has not allocated required choices |
89 | Keeper download failed |
90 | User disabled scanner |
91 | Bus Off detected on scanner |
92 | No network power detected |
93 | CRC failure detected on one or more configuration blocks |
94 | Reserved |
95 | Scanner application program flash is being updated |
96 | Port is in test mode operation |
97 | User halted scanner |
98 | Esc, Overflow, Divide or other processor error |
99 | Scanner watchdog has timed out |
Provide Feedback