Assign variables
Use the variable selector to assign an existing variable to a Program Organization Unit (POU) element of a ladder diagram (LD) or function block diagram (FBD) program.
Prerequisites
- The POU is not empty.
To assign variables
- InProject Organizer, locate the POU, and then double-click the POU.
- Open the variable selector by doing one of the following:
- Double-click the variable, and then select
. - Right-click the variable, and then selectSelect variable.
- Select a variable to assign by doing one of the following:
- Select the variable, and then selectSelect.
- Double-click the variable.
Provide Feedback