Cross-reference browser
The cross-reference browser is a search tool for finding the logic references to variables within the
Micro800
project.Open the cross-reference browser from:
- The language editor of a ladder diagram, function block diagram, or structured text program.
- The global or local variable grid.
The cross-reference browser displays references to the variable based on where the variable is used, including:
- Ladder diagram programs
- Structured text programs
- Function block diagrams
- User-defined functions
- User-defined function blocks
- Controller configurations
The cross-reference browser shows the following information about the variable:
- Name: The variable name that is referenced in the controller project.
- Instruction: The name of the instruction in which the variable is used.
- Location: The location where the variable is used and a link to the location.
- Access: The communication access to the variable asNo Access,Read/Write, orRead.
Cross-reference browser

Item | Description |
|---|---|
![]() | Displays the location of the variable in the controller project:
It is read-only. |
![]() | Refreshes the cross-reference list. Refresh is used after:
|
![]() | Displays the total number of references to the selected variable. |
![]() | Opens the unused variable selector to view the user-defined variables that are not assigned to a controller program. |
![]() | Expands or hides the reference information for the category. |
![]() | Displays the location of the reference in Project Organizer . |
Provide Feedback