Quick declaration variable settings
Category | Setting | Description |
|---|---|---|
Name | Prefix | The first part of the variable name that appears before the number value The naming conventions are as follows:
|
From | The starting value for the first variable The From value must be smaller than the To value.The value is from 0 through 99998. | |
To | The ending value for the last variable The To value must be larger than the From value.The value is from 1 through 99999. | |
Suffix | The last part of the variable name that appears after the number value The naming conventions are as follows:
| |
Attributes | Data type | The type of the variable Supported types are:
For information about data types, see Data types overview. |
Direction | The role of the variable as input, output, or internal Options are:
This parameter is available for the local variables of user-defined functions or user-defined function blocks. | |
String size | The length of a string variable, which applies to the STRING data type The size is from 1 through 255. |
Provide Feedback