Indirect bit addressing
Use a SINT variable to perform indexed bit addressing on 8-bit, 16-bit, 32-bit, and 64-bit integers or words in
Micro800
controller programs using the syntax of Var1.[Var2]
.For consistency, the indirect bit addressing syntax also supports using a defined word or constant in place of
Var2
, which results in direct bit addressing.
TIP:
- For indirect bit addressing, if the value of the variable used for the bit index is out of range at runtime, a controller fault occurs.
- Direct bit addressing is supported in all versions using the syntaxVar1.Constant, whereConstantis an integer from 0 through 63.
Integer Type | Range |
|---|---|
8-bit integer | From 0 through 7 |
16-bit integer | From 0 through 15 |
32-bit integer | From 0 through 31 |
64-bit integer | From 0 through 63 |
Example: Indirect bit addressing syntax
Var1.[Var2]
The example uses a SINT variable as the index.
Var1 is a UDINT variable. Each bit can be referenced as a Boolean by using Var 2, a SINT variable, to index through the Booleans.
Example: Direct bit addressing syntax
MyInteger.[3] MyInteger.[MY_DEFINED_WORD]
Provide Feedback