Add bit-level comments to a variable
Bit-level comments are created in the variable grid and displayed with the variable name in the language editor. The comments are stored in the controller project and saved in plaintext format.
To add bit-level comments to a variable
- In the global or local variable grid, locate the variable to which you want to add the bit-level comments.
- In theCommentcolumn, enter the bit-level comments, and then select theEnterkey.In the language editor, after assigning a variable with bit-level comments to an element, the comments will appear above the variable or as a tooltip.TIP: To delete bit-level comments, in theCommentcolumn, delete the comments, and then select theEnterkey.
Provide Feedback