Ethernet device settings
After adding an Ethernet device, a
<device-name>
node is created under Ethernet
in Project Organizer
. To view and configure the Ethernet devices, do one of the following:- Double-click the node.
- Right-click the node, and then selectProperties.
The settings displayed on the
<device-catalog-number: device-name>
page vary with type of the device that you added.Setting | Description |
|---|---|
Information - Overview | Displays:
|
Settings in the Devices definition dialog | |
Device type | Displays the catalog number of the added device. It is read-only. |
Name | Displays the device name that you entered. The name must be unique. Do not set a name using the device type because it contains reserved words. We recommend that you attach a number to the device type. For example, powerflex523_1. |
Description | Displays the additional information about the device. It is optional. |
Ethernet address | Specifies the IP address of the added device. The default address is 1.1.1.1. |
Revision | Displays the device revision, comprising a major revision number followed by a minor revision number.
|
Electronic keying | Displays the selected electronic keying option. Electronic keying reduces the possibility of using an incorrect device in the control system by comparing the device specified in the project with the installed device. The available options vary with the selected device type:
|
Mode | Specifies the device operating mode. Options include:
The setting is available for the PowerFlex® 525-EENET and PowerFlex 525-E2P device type. |
Drive rating | Lists the power rating with global voltage classes of the drive. It is available when you select a PowerFlex drive. |
Configuration - Connection | |
Requested packet interval | Specifies the connection update rate. The connection transfers data to or from the device at least as frequently as specified. The value is from 5 through 9999.9. The default value is 20.0. The range for Kinetix® 5100 is from 5 through 3200.The setting is configurable when the controller is online. |
Unicast connection over EtherNet/IP | Determines whether to use a unicast connection over EtherNet/IP or multicast connections. The setting is configurable when the controller is online. |
Inhibit module | Determines whether to inhibit the connection to the module. The setting is configurable when the controller is online. |
Major fault on controller if connection fail while in run mode | Enables the controller to check the Class 1 communication with the device when switching from Program to Run mode. If connected, the controller enters Run mode. Otherwise, the 0xF8A4 fault occurs. |
Connection - Connection fault | Shows the connection fault information if any while online. |
Configuration - Comm config | |
Communication format | Specifies the device communication format. The setting is available for generic devices. The selected communication format for an I/O module determines how the module communicates with the controller, which configuration pages are available, and the tag structure and configuration method that you will use to configure the module. Specifically, the communication format determines:
|
Provide Feedback