Online settings
Use the
Online settings
dialog to configure the controller's settings for communication, downloading, uploading, and device discovery.Category | Setting | Description |
|---|---|---|
General | Use Cellular Network | Determines whether to use the cellular network for downloading and uploading.
The default setting is No . |
Download | Mode | Sets the controller mode when downloading is completed.
The default setting is Remote program . |
Connection | Determines whether to connect to the controller when downloading is completed.
The default setting is Connect . | |
Project value | Determines whether to download the values of the variables.
The default setting is No . | |
Warning | Determines whether to download the controller project that contains build errors.
The default setting is Yes . | |
Communication | Determines whether to download the project when the driver settings for Ethernet, USB, or DF1 differ in the controller and the project. The controller cannot automatically establish a connection if you download mismatched configurations between the controller and the project. The default setting for Download Ethernet is No .The setting is applicable when using the same driver to download the corresponding driver settings for Ethernet, USB, or DF1. The default setting for Download Ethernet , Download USB , or Download Serial Port is No . | |
Upload | Connection | Determines whether to connect to the controller when uploading is completed.
The default setting is Connect . |
Project value | Determines whether to upload the values of variables.
The default setting is No . | |
Discover | Discover | Determines whether to connect to the controller and initiate debugging when discovery is completed.
The default setting is Connect . |
Provide Feedback