View panes
Use the
View
menu to display or hide specific panes. The location, pinned status, and visibility of panes are reserved after closing and reopening FactoryTalk Design Workbench
.Select | To |
|---|---|
Pin the selected pane to the current location. | |
Unpin the selected pane. | |
Hide the content of the selected pane. | |
Display the content of the selected pane. | |
Close the selected pane. | |
Left panes | Display or hide the panes that are last pinned to the left side of the user interface (UI). |
Right panes | Display or hide the panes that are last pinned to the right side of the UI. |
Bottom panes | Display or hide the panes that are last pinned at the bottom of the UI. |
Reset layout | Restore panes to their default locations, pinned status, and visibility. |
Project organizer | Display or hide Project Organizer . Project Organizer is pinned to the left side of the UI by default. |
Properties | Display or hide Properties . The pane is pinned to the lower right of the UI by default. |
Toolbox | Display or hide Toolbox . The pane is pinned to the upper right of the UI by default. |
Connection | Display or hide Connection . The pane is hidden by default. |
Display Output with the Console page opened. | |
Display Output with the Error list page opened. | |
Display Output with the Log page opened. |
Provide Feedback