Loading
Press Release
Recent ActivityRecent Activity

Rockwell Automation Joins Initiative to Bring OPC UA to Field-Level Devices

Rockwell Automation is joining an OPC Foundation initiative to extend the OPC UA protocol to field-level industrial communications

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail
Press Release
Recent ActivityRecent Activity
Rockwell Automation Joins Initiative to Bring OPC UA to Field-Level Devices
Rockwell Automation is joining an OPC Foundation initiative to extend the OPC UA protocol to field-level industrial communications

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

Under the initiative, a series of working groups are being formed to bring the OPC UA protocol’s vendor-independent, end-to-end interoperability to field-level devices. The initiative plans to address use cases not currently in scope for EtherNet/IP. It could also simplify other use cases, especially in multi-vendor, controller-to-controller environments and for the vertical integration of field devices.

“Rockwell Automation has always supported the development and use of open standards,” said Paul Brooks, business development manager, Rockwell Automation. “Extending the OPC UA protocol to the field level or shop floor can help simplify system development and accelerate a company’s journey to a Connected Enterprise.”

As the primary author of the EtherNet/IP specifications, Rockwell Automation understands EtherNet/IP users may see compatibility risks in technology developed for a different ecosystem. The company intends to mitigate these risks through both its ongoing development of EtherNet/IP and its intentions for the OPC UA protocol.

Rockwell Automation’s priorities within the new OPC Foundation initiative include working to help ensure the following:

  • OPC UA specifications are written with the same level of rigor and completeness as the EtherNet/IP specifications.

  • Time-sensitive networking (TSN) is commonly applied across the OPC UA, EtherNet/IP and PROFINET protocols, so all three can coexist on a common TSN-based network.

  • OPC UA pub/sub technology is implemented in a way that allows existing EtherNet/IP installations to support OPC UA devices.

  • OPC UA hardware requirements allow the protocol to be deployed on hardware platforms that are common in today’s EtherNet/IP components.

  • OPC UA software requirements allow the protocol to be deployed within current EtherNet/IP-centric software tools without significant changes to user workflows.

  • Conformance test practices mandated for EtherNet/IP reflect the necessary requirements for OPC UA conformance testing.

“We are committed to these priorities to help make sure EtherNet/IP users have a choice of whether and when they migrate to the new OPC UA protocol,” Brooks said. “We want users to determine the pace of this migration based on the value that they receive, rather than technology choices made in the specification. We trust that others engaged in the initiative will share this common goal.”

Published December 11, 2018


Susanne Bergmann
Susanne Bergmann
Field Marketer, Germany, Rockwell Automation
Connect:
EmailEmail
Zhongjie Li
Zhongjie Li
Competency Center Manager, Rockwell Automation
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right