Loading
Press Release | October 27, 2020
Recent ActivityRecent Activity

Rockwell Automation Introduces Next Generation Edge Gateway to Accelerate IT/OT Convergence

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

FactoryTalk® Edge Gateway™ accelerates edge to cloud digital transformation and unlocks higher value business insights at enterprise level

MILWAUKEE--(BUSINESS WIRE)-- Today, Rockwell Automation introduced the first capability of its edge strategy with FactoryTalk Edge Gateway, to simplify and accelerate IT/OT convergence. Industrial enterprises struggle to aggregate operational data from heterogeneous sources and add relevant context from the source—such as process conditions, time stamps, machine states and other production states—to the IT layer. This prevents them from uncovering potentially game-changing insights at the enterprise level. While traditional gateway solutions fail to address these important challenges, FactoryTalk Edge Gateway goes a step above to not only enrich OT data with critical context where it matters the most—at the edge—but also delivers it in a flexible common information model to IT applications, so that industrial enterprises can derive critical insights for a competitive edge.

This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20201027005455/en/

(Graphic: Business Wire)

FactoryTalk Edge Gateway is an important foundation of a broader edge platform offering that will include elements of pre-built data analytics models, machine learning, tailored applications, and scalable compute. It is the latest addition to the highly recognized and widely adopted FactoryTalk® Analytics suite offering that addresses diverse industries and Industrial IoT (IIoT) use cases. FactoryTalk Edge Gateway is also a key pillar in Rockwell Automation’s strategy to accelerate digital agility across the industrial devices to cloud spectrum with partnerships, including PTC and Microsoft.

Today, industrial facilities are made up of heterogeneous systems and devices that generate voluminous data at very high speeds—resulting in significant data silos. Connecting the dots across these industrial data silos by building relevant OT data context is critical for generating higher value actionable insights. Furthermore, unless the industrial OT data is packaged into a logical data model that both IT and OT applications can understand, IT/OT convergence remains a farfetched prospect.

A leading Fortune 100 pharmaceuticals manufacturer says, “Legacy systems today are not IIoT enabled and need many different software programs to collect and organize data. With existing methods, the operational attribute values collected have different timestamps, so it is impossible to synchronize the data together. Compared to that, FactoryTalk Edge Gateway automatically stitches the data together and puts it in a payload using pre-configured information model hierarchy. It gives one solution to collect and organize the relevant data.”

FactoryTalk Edge Gateway’s unique data management capabilities result in up to a staggering 70% reduction in analytics data preparation efforts for data scientists or analysts, while providing higher quality OT data. The underlying common information data model is orchestrated by the unique Rockwell Automation FactoryTalk® Smart Object™ capability and can be efficiently mapped to on-premises or cloud applications to generate predictive insights across the enterprise. FactoryTalk Edge Gateway is designed to integrate with best-in-class ecosystem solutions like Microsoft Azure and FactoryTalk® InnovationSuite™, powered by PTC, and a variety of big data, IIoT, and cloud applications.

“Industrial businesses need actionable enterprise-level insights to achieve their goals. As customers continue to drive IT/OT integration and leverage operational data to drive insights, they are realizing that having the right OT data context is critical to scale their digital transformation initiatives,” said Arvind Rao, Director, Product Management for Information Systems at Rockwell Automation. “With FactoryTalk Edge Gateway, we are dramatically reducing the time and effort required to build, maintain and enrich this critical OT context. This provides our customers with the opportunity to realize double-digit operational improvements through analytics.”

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 23,000 problem solvers dedicated to our customers in more than 100 countries. To learn more about how we are bringing The Connected Enterprise to life across industrial enterprises, visit www.rockwellautomation.com.

FactoryTalk and InnovationSuite are trademarks of Rockwell Automation Inc.

View source version on businesswire.com: https://www.businesswire.com/news/home/20201027005455/en/

Chaya Jacobs
Rockwell Automation
414-382-0501
CJacobs@ra.rockwell.com

Source: Rockwell Automation, Inc.

Published October 27, 2020


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation Introduces Next Generation Edge Gateway to Accelerate IT/OT Convergence