Loading
Press Release | August 18, 2014
Recent ActivityRecent Activity

First On-Machine Switch From Rockwell Automation Simplifies Network Design, Integration

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

ArmorStratix 5700 switch extends portfolio to the on-machine space for connectivity in harsh environments

MILWAUKEE, Aug. 18, 2014 - Rockwell Automation has announced the launch of the Allen-Bradley ArmorStratix 5700, its first on-machine switch. Built with ruggedized IP67 protection, the Layer 2 managed industrial Ethernet switch can be mounted directly onto a machine or application, reducing the overall size and cost of a control cabinet, and shrinking the machine footprint.

“In many applications, cabinet space for system-level networks is limited or nonexistent,” said Mark Devonshire, product manager for Stratix switches, Rockwell Automation. “The ArmorStratix 5700 switch expands the Allen-Bradley  offering from Rockwell Automation – an industrially hardened portfolio of products that requires no cabinetry – and leverages pre-configured, quick-connect systems and simplified wiring layouts to reduce installation, troubleshooting and maintenance activities.”

Senior analyst with ARC Advisory Group comments: “Machine-mounted Ethernet switches with M12 connectors and IP67 ratings are very popular among machine builders. The new ArmorStratix 5700 switch is a joint Rockwell Automation-Cisco developed product that includes these features along with Cisco IOS. This robust, machine-mounted switch is a new development that should go a long way toward resolving the information technology/operational technology struggles in manufacturing plants today.”The ArmorStratix 5700 managed switch advances connected enterprise goals by delivering integration of machine-level data that, due to cost or location, would otherwise remain isolated from business-level systems. Using the Cisco IOS network infrastructure software, this switch manages the transfer of production data to enterprise-level databases and information systems for improved decision making.

This industrial switch simplifies the design and development of machine-level networks through configuration and monitoring tools. These tools help enable easy setup and diagnostics from within the Rockwell Automation Integrated Architecture system – bridging the gap between IT and the automation engineer.

News Release AssetsThe ArmorStratix 5700 Layer 2 switch offers high availability, Quality of Service (QoS), and automated monitoring to help simplify network optimization and convergence. The switch comes standard with 8, 16 and 24 fixed-port configurations, and each base model comes with M12 Ethernet connectors, SD flash card, dual-power inputs and a panel-mounted design. An expanded ArmorStratix 5700 switch offering includes 10 and 18 fixed-port configurations, with 2 gigabit ports, hardware-based IEEE 1588, hardware alarms, and up to eight Power over Ethernet (PoE) ports.

About Rockwell Automation 

Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,000 people serving customers in more than 80 countries.


Media Contacts
Tiffany Pfremmer
Rockwell Automation
414.839.7425
tbockhop@ra.rockwell.com


Media Contacts
tbockhop@ra.rockwell.com

Marnie Kopischke
PadillaCRT
612.455.1737
marnie.kopischke@padillacrt.com


Allen-Bradley, ArmorStratix 5700, Integrated Architecture, LISTEN. THINK. SOLVE., On-Machine and Stratix are trademarks of Rockwell Automation Inc.
Cisco IOS is a trademark of Cisco.


 

Published August 17, 2014


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left First On-Machine Switch From Rockwell Automation Simplifies Network Design, Integration