Downloads
What is this for?
Used to visualize vibration and temperature (taken at the same measurement point) and to manage the corresponding alarms.
General Characteristics
This development includes the following:
- Program configuration in Studio 5000
- HMI screen setup in FactoryTalk Optix
Advantages:
- Provides an initial reference for condition monitoring developments of rotating machines
- Enable monitoring of the system, even remotely.
Limitations/Disadvantages
- It is limited to acceleration and temperature readings acquired through the Dynamix 1444
Is this useful for me?
If you need to implement a panel to monitor the vibration and temperature of rotating machines
Application Areas - It can be applied in condition-based monitoring environments for rotating machines.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
How to get it working?
Requirements: products, tools, prior knowledge.
Hardware
- Any Logix Controller
- Any Optix Panel or PC
- Dynamix 1444
Software
- Studio 5000 (the program was developed in version 38)
- FactoryTalk Optix (application developed using version 1.6)
Knowledge
- Basic knowledge of programming and configuration in:
- Studio 5000
- Factorytalk Optix
- Vibration Analysis
Implementation Guide
Step 01
Studio 5000 Program
- Step 1.1
- Step 1.2
- Step 1.3
- Step 1.4
- Step 1.5
3. Configure the 1444 module
a) Add the 1444-DYN04-01RA module
b) Configure the module personality according to the specific needs of the application.
c) We will work with a dual accelerometer 1443-ACC-AT-T, but the procedure is similar for accelerometers that include temperature measurement from other brands.
4. We will configure the AOP according to a typical centrifugal pump application, using the application document 1444-AT001 as a reference for the case ‘Pumps – Horizontal Mount’
a) Connection b) Speed c) HW Configuration d) Filters |
e) Overall f) FFT g) Bands h) Temperature configuration |
5. We will configure the alarms within the 1444 module.
Step 02
FactoryTalk Optix Development
FactoryTalk Optix: Condition Monitoring Dashboards
Version 1.0 - January 2026