Downloads
What is this for?
The Mettler Toledo IND360 product is a product for accurate weight measurement (load cell) and allows excellent integration with our controllers (ControlLogix, CompactLogix) via Ethernet/IP. The partnership between Mettler Toledo and Rockwell Automation has allowed the development of libraries such as Add-on, Faceplates (HMI), sample codes, to make integration easy and fast. With the Application Code Manager feature (code generator and screens) it is possible to integrate, generate controller application code (Studio 5000), generate HMI screens and network configurations, reducing setup time and startup of production lines and industrial machines.
https://www.mt.com/us/en/home/library/case-studies/industrial-scales/Encompass.html
- General Characteristics
- Advantages
- Limitations and Disadvantages
Our Device Object Libraries allow you to easily interact with Rockwell Automation® Intelligent devices, as drives, motion, network switches, sensors, IoT, and more. The libraries contain tests, documented, and lifecycle. Managed objects that can be used with the manufacturer of machines, processes, and libraries packaged or as stand-alone components. Device Objects Include HMI Faceplates para FactoryTalk® View ME/SE e Studio 5000 View Designer® software and provide a user interface that integrates seamlessly with the goods.
HMI faceplates are standard display files that provide the average user with Interface. These are HMI pop-up screens used to display detailed information related to a specific instruction or device. On systems that follow ISA 101.1 According to design guidelines, front-facing displays are often referred to as Level 4 monitors.
Preconfigured device objects include a supplemental instruction line and a HMI front panel that offers the following benefits:
- Collect, process, and deliver data between smart devices and Application Logic
- Detailed collection and delivery of device data
- Improved device status and diagnostics
- Common control interfaces that maximize device automation flexibility Selection and reuse of application code
Device objects use cases:
- Basic device maintenance and diagnostics
- Virtual device operations for start-up and commissioning
- Operator and program control for machines and processes Applications
Integration via Ethernet/IP allows for excellent ease of integration, reducing time and line start-up process. Use of Application Code Manager to generate controller code (Add-on) and general configurations and construction of HMI faceplates for integration.
Application Code Manager
Studio 5000® Application Code Manager is a tool that can be used with Device Object libraries to speed up the development of projects and machines. This volume Coding tool allows you to easily design and standardize functionalities with Reusable application code. Enable more efficient project development with reusable code libraries:
- Quickly create and deploy projects through our app content
- Libraries - Import Rockwell-sourced application content libraries for agility system development.
Number of IND-360 devices, integrated via Ethernet/IP, depends on the limitation of CIP connections of each controller used.
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
Is this application relevant to me?
Integration via Ethernet/IP allows excellent ease of integration, reducing time and start-up of lines, process and industrial machines.
How can I make it work?
Requirements: products, tools, prior knowledge.
Hardware
- PanelView™ 5500 with v8 or later firmware
- PanelView™ Plus with v10 or later firmware
- ControlLogix® 5570/5580 controller or CompactLogix™ 5370/5380
- Controller with v3.01 or later firmware
Software
- Studio 5000 Logix Designer® v31.02 or later for PAC Application Development
- Studio 5000® Application Code Manager v4.01 and later for bulk code configuration
- Studio 5000 View Designer® v8.00 and later for PanelView™ 5000 Application Development
- FactoryTalk® View Studio v10 and later for PanelView™ Plus or
- FactoryTalk® View SE Application Development
Prior Knowledge
- SO Windows
- Studio 5000 Design Studio and View Design
- FactoryTalk View Studio ME
- FactoryTalk View Studio SE
- Application Code Manager - Basic
Implementation Guide
- Step 01
- Step 02
- Step 03
- Step 04
- Step 05
Manual de Referência: DEVICE-RM905A-EN-P.pdf
Localizado em General_Files.zip, no caminho:
MettlerToledoDeviceLibrary_v1.00.00\Reference Manual\DEVICE-RM905A-EN-P.pdf
Como importar e configurar objetos de dispositivo Metter Toledo no ACM – Application Code Manager.
How to Import and Configure Metter Toledo Device Objects in Studio 5000 Logix Design.
How to Import and Configure Metter Toledo Device Objects in FactoryTalk View ME and SE.
How to Import and Configure Metter Toledo Device Objects in Studio 5000 View Design.
MT-IND360 Visualization & Operational Data - Faceplates.
Ease of integrating a MT IND360 weight indicators via Ethernet/IP
Version 2.0 - October 2026