11:30 a.m. - 12:30 p.m. Singapore Time (GMT+8)
9:00 a.m. - 10:00 a.m. India Standard Time (GMT+5:30)
14:30 p.m. - 15:30 p.m. Australian Eastern Daylight Time (GMT+11)
16:30 p.m. - 17:30 p.m. New Zealand Daylight Time (GMT+13)
Data is only as valuable as the analytics behind it and the actions it drives!
The convergence of data and analytics with industrial operations have made Industrial DataOps a necessity. Complex industrial data requires context if it is to be used broadly in an organization. A central, contextualized source of truth with automated data pipelines provides industrial users a common and simplified way to discover, understand and analyze industrial data.
In this webinar our experts will demonstrate how FactoryTalk DataMosaix can extract data from common industrial data sources, build meaning through contextualization, perform ad-hoc analytics and create scalable applications.
Learn how you can start with foundational, quick-win use cases that drive operational value while also progressing to advanced, high impact predictive and prescriptive applications.
Register today!