Predictive Maintenance

PowerFlex®
750-Series Products with
TotalFORCE®
Control contain algorithms for predictive maintenance that are used to improve the uptime of machines, processes, and facilities. These algorithms monitor the lifespan of certain components and display the percentage of remaining life and the number of hours or counts of remaining life in specific parameters or a software interface. These algorithms can be used to alert personnel when the components are nearing the end of their lifespan so the components can be replaced before they fail. For an overview of predictive maintenance, see the Predictive Maintenance section in the PowerFlex 750-Series Products with TotalFORCE Control Reference Manual, publication 750-RM100.
IMPORTANT: Failure to address predictive maintenance alarms can cause unexpected downtime or premature product failure.
For firmware revisions 6.005 and earlier, the remaining life of components with predictive maintenance appear in parameters. For firmware revisions 10.001 and later, the remaining life of components with predictive maintenance appear on the Predictive Maintenance page in the Device Details window in
Connected Components Workbench software
software and the Drive Details window in
Studio 5000 Logix Designer®
application (as shown in this Predictive Maintenance page example).
NOTE: Firmware revisions 6.xxx and earlier cannot be used in frame 6L and 7L liquid cooled drives.
Connected Components Workbench - Predictive Maintenance Page
An example of the CCW Predictive Maintenance page that shows the remaining life of components in a PowerFlex 755T product
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal