Important User Information
Read this document and the additional resources on installation, configuration, and
operation before installing, configuring, operating, or maintaining this product. Users must
understand the installation, wiring instructions, and all applicable codes, laws, and
standards.
Installation, adjustment, commissioning, use, assembly, disassembly, and maintenance must
be performed by properly trained personnel with applicable codes of practice. Using this
equipment in a manner not specified by the manufacturer may adversely impair the protection
it provides.
Rockwell Automation, Inc. is not liable for indirect or consequential damages potentially
resulting from the use or application of this equipment.
Seller warrants that new hardware Products furnished hereunder will be free from defects in
material, workmanship, and design for a period of one (1) year from the date of the invoice
from Seller or its appointed distributor. To review the current terms and conditions of
sale, see rok.auto/terms-of-sale.
Examples and diagrams in this manual are for illustrative purposes only. Because
installation requirements vary, Rockwell Automation, Inc. assumes no responsibility for the
actual future use of products based on these examples.
Rockwell Automation, Inc. assumes no patent liability for the use of information, circuits,
equipment, or software described in this manual.
Reproduction of this manual, in whole or in part, without the written permission of
Rockwell Automation, Inc., is prohibited.
Safety-related notes are included throughout this manual where applicable.
WARNING:
Identifies information about practices or circumstances that can cause an explosion in
a hazardous environment, which may lead to personal injury or death, property damage, or
economic loss.
ATTENTION:
Identifies information about practices or circumstances that can lead to personal
injury or death, property damage, or economic loss. Attentions help you identify a
hazard, avoid a hazard, and recognize the consequence.
IMPORTANT:
Identifies information that is critical for successful application and understanding of
the product.
These labels may also be on or inside the equipment to provide specific precautions.
SHOCK HAZARD:
Labels may be on or inside the equipment, for example, a drive or motor, to alert
people that dangerous voltage may be present.
BURN HAZARD:
Labels may be on or inside the equipment, for example, a drive or motor, to alert
people that surfaces may reach dangerous temperatures.
ARC FLASH HAZARD:
Labels may be on or inside the equipment, for example, a motor control center, to alert
people to potential Arc Flash. Arc Flash will cause severe injury or death. Wear proper
Personal Protective Equipment (PPE). Follow ALL Regulatory requirements for safe work
practices and for Personal Protective Equipment (PPE).
The following icon may appear in the text of this document.
TIP:
Identifies information that is useful and can help to make a process easier to do or
easier to understand.
Rockwell Automation recognizes that some of the terms that are currently used in our
industry and in this publication are not in alignment with the movement toward inclusive
language in technology. We are proactively collaborating with industry peers to find
alternatives to such terms and making changes to our products and content. Please excuse the
use of such terms in our content while we implement these changes.
Provide Feedback