Remove and Install the AC Common Mode Filter Circuit Board for Frame 7
Replace the AC common mode filter circuit board with kit catalog number SK-RM-EMCFB1. Follow these steps to remove and install the AC common mode filter circuit board.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Open the enclosure door.
- Remove the protective guard. See Remove and Install the Protective Guard for Frame 7.
- IMPORTANT: The PE-A2 jumper on the new AC common mode filter circuit board must be installed in the same position as the old board.
- Record the position of the PE-A2 jumper on the circuit board.ItemDescriptionAPE-A2 jumper in the "IN" positionBPE-A2 jumper in the "OUT" position
- Disconnect the PE-A2 jumper wire from the wire stake on the board.
- Remove the five, M4 x 16 mm slotted-Torx screws that secure the circuit board to the sheet metal panel and remove the board.
- Repeat steps 5…7 for each AC common mode filter board.
- Install the AC common mode filter circuit board in the reverse order of removal.
- Verify that the PE-A2 jumper is installed in the same position on the new board as it was on the old board.
Provide Feedback