Remove and Install the AC Precharge Time Delay Relay for
Frame 7L

Replace the AC precharge time delay relay with kit catalog number 20-750-MACPC-TDR. Follow these steps to remove and install the AC precharge time delay relay.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Open the enclosure door.
  4. Remove the protective guard.
  5. TIP: The AC precharge time delay relay is located behind the control pod and on the back of the AC precharge components panel.
  6. Open the AC precharge components panel. See Open and Close the AC Precharge Components Panel for Frame 7L.
  7. Disconnect the wires from the terminals on the time delay relay.
    example of how to remove the AC precharge time delay relay wire connections for a frame 7 and 7L drive
  8. Remove the two M4 x 14 mm slotted-Torx screws that secure the time delay relay to the panel and remove the relay.
    example of how to remove the AC precharge time delay relay fora frame 7 and 7L drive.
  9. Install the AC precharge time delay relay in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal