Remove and Install the Stirring Fan Assembly for Frame 6

Replace a stirring fan assembly with kit catalog number SK-RM-MFAN1-F6. Follow these steps to remove and install the stirring fan assembly.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Remove the cover from the chassis. See Remove and Install the Frame 6 Cover.
  4. Disconnect the fan power wire harness connectors (A) from the connectors on the chassis.
  5. Loosen the M4 captive screw that secures each of the fan assemblies to the chassis.
  6. Slide the fan assembly away from the chassis until the mounting tabs (B) align with the holes in the fan mounting plate, and remove the fan assembly.
    example of how to remove the frame 6 stirring fan assembly
  7. Install the stirring fan assembly in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal