Remove and Install the Heatsink Fan Assembly for Frame 5

Replace a heatsink fan assembly with kit catalog number SK-RM-HSFAN1-F5. Follow these steps to remove and install the heatsink fan assembly.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Loosen the two captive screws that secure the fan assembly to the chassis.
  4. Carefully pull the bottom of the fan assembly away from the chassis and release the three tabs from the chassis. The power wire harness is connected inside the chassis.
    example of how to remove the frame 5 heatsink fan assembly
  5. Disconnect the fan wire harness connector P2 from connector J2 inside the chassis and remove the fan assembly.
    example of how to disconnect the frame 5 heatsink fan assembly wire harness from the drive
  6. Install the heatsink fan assembly in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal