Remove and Install the Protective Guard for Frames 7 and 7L
You must remove the protective guard to access certain components in the enclosure. Follow these steps to remove and install the protective guard.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Open the enclosure door.
- If a door-mounted HIM is installed, cut the cable tie (A) that secures the HIM communication cable to the guard.
- Loosen the 16 M5.5 x 13 mm Torx screws that secure the guard to the enclosure and remove the guard. It is not necessary to remove the screws.
- IMPORTANT: Be sure to secure the HIM cable to the guard with a new cable tie.
- Install the protective guard in the reverse order of removal.
Provide Feedback