Remove and Install the LCL Filter/Power Module Heatsink Fan Assembly for Frame 7

Replace an LCL filter/power module heatsink fan assembly with kit catalog number SK-RM-MFAN-F7. Follow these steps to remove and install the LCL filter/power module heatsink fan assembly.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Open the enclosure door.
  4. Below the fan assembly, reach through the opening in the front of the power or LCL filter module chassis, and disconnect the fan power supply connector P4 from J4 on the fan assembly.
    example of how to disconnect the frame 7 LCL filter or power module heatsink fan
  5. Loosen the four captive M5 screws on the front of the fan assembly and slide the assembly out of the chassis.
    example of how to remove the frame 7 heatsink fan assembly
  6. Install the LCL filter/power module heatsink fan assembly in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal