Remove and Install the LCL Filter Capacitor - Frame 6L

Replace an LCL filter capacitor with kit catalog number SK-RM-LCLCP4-F6L.
Follow these steps to remove the LCL filter capacitor.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Remove the four M5 x 12 mm slotted-Torx screws that secure the top cover to the lower chassis and remove the cover.
    example of how to remove the frame 6L liquid cooled drive top cover.
  4. Remove the four M5 x 12 mm slotted-Torx screws that secure the capacitor assembly to the chassis.
  5. Cut the two cable ties (A) that secure the capacitor to the bracket and discard the cable ties.
    example of how to remove the frame 6L liquid cooled drive LCL filter capacitor screws
  6. Remove the three M8 hexagonal nuts that secure the capacitor wires to terminals R, S, and T at the top of the capacitor and remove the wires.
    example of how to remove the frame 6L liquid cooled drive LCL filter capacitor nuts from the capacitor terminals
  7. Remove the capacitor and support bracket assembly from the drive.
    example of how to remove the frame 6L liquid cooled drive LCL filter capacitor and support bracket
  8. Insert the stud on new capacitor into the hole in the support bracket and secure the capacitor to the bracket by using an M12 hexagonal nut.
    example of how to install the frame 6L liquid cooled LCL filter capacitor on the support bracket
  9. Insert the cable ties into the notches in the chassis mounting plate. Do not tighten the cable ties.
    example of how to install the frame 6L liquid cooled drive LCL filter capacitor cable ties
  10. Align and tighten the three M8 hexagonal nuts that secure the capacitor wires to terminals R, S, and T at the top of the capacitor assembly.
  11. Place the capacitor assembly into the cable ties in the chassis and align and tighten the four M5 x 12 mm slotted-Torx screws that secure the capacitor assembly to the chassis.
    example of how to install the frame 6L liquid cooled drive LCL filter capacitor
  12. By tightening the cable ties (A), secure the capacitor to the mounting plate.
    example of how to secure the frame 6L liquid cooled drive LCL filter capacitor to the mounting plate by tightening the cable ties
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal