Remove and Install the Control Pod HIM Cradle with DPI Connector (XT) for Frame 6L
Frame 6L
Replace the control pod human interface module (HIM) cradle with
DPI™
connector (XT) with kit catalog number SK-RM-CR1.Follow these steps to remove and install the control pod HIM cradle with
DPI™
connector.- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis.
- If a HIM is installed in the control pod cradle, remove the HIM.
- If used, disconnect theDPI™cable (A) from the connector on the bottom of the HIM cradle.TIP: If a cable is not connected to theDPI™port on the human interface module (HIM) cradle, be sure to leave the protective cover installed.
- Loosen the screw that secures the HIM cradle to the pod chassis, and rotate the cradle up to a 90° horizontal position.
- Disconnect the terminal block (B) for the HIM wire harness from the connector on the main control board.
- TIP: If a cable is not connected to theDPI™port on the HIM cradle, be sure to leave the protective cover installed.
- Press in on the tabs at the top of the HIM cradle where it connects to the control pod chassis to release the cradle from the chassis.
- IMPORTANT: Do not remove protective covers (C) from wire harnesses, circuit board connectors, terminal blocks, and fiber-optic transceivers and ports unless used at the time of installation. For the product to meet the corrosive atmosphere rating, protective covers must remain installed in unused connectors during storage and operation.
- Install the control pod HIM cradle withDPI™connector in the reverse order of removal.
Provide Feedback