Remove and Install the Fan Power Supply Circuit Board for Frame 5

Replace a fan power supply circuit board with kit catalog number SK-RM-PSB1-F5-F6. Follow these steps to remove and install the fan power supply circuit board.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Remove the cover from the chassis. See Remove and Install the Frame 5 Cover.
  4. Disconnect these cable connectors from the fan power supply circuit board:
    • P1 from J1
    • P2 from J2
    example of the frame 5 fan power supply circuit board connections locations
  5. Remove the six M4 x 10 mm Torx screws that secure the fan power supply circuit board to the bracket and remove the board.
    example of how to remove the frame 5 fan power supply circuit board from the drive chassis
  6. Install the fan power supply circuit board in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal