Remove and Install the Control Pod (Standard) for Frames 8...15
Replace the control pod (standard) assembly with kit catalog number 20-750-MCPOD1-F8M or 20-750-MCPOD2-F8M. Follow these steps to remove and install the control pod.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Open the enclosure door.
- If a human interface module (HIM) is installed in the HIM cradle, remove the HIM.
- Remove the fiber-optic cables from the cable management devices (A in illustration) in the control pod.
- IMPORTANT: The minimum inside bend radius for fiber-optic cable is 50 mm (2 in.). Any bends with a shorter inside radius can permanently damage the fiber-optic cable. Signal attenuation increases as inside bend radius is decreased.TIP: It is easier to remove the fiber transceiver circuit board from the pod before removing the fiber-optic cables. However, it is possible to remove the fiber-optic cables without removing the boards.
- Loosen the two captive thumbscrews that secure each of the fiber transceiver circuit boards to the chassis and remove the boards with cables. Retain the fiber transceiver boards for reuse.
- TIP:The control pod is shown separated from the enclosure to clarify the instructions only.
- Remove the fiber-optic cables from the applicable ports on the fiber transceiver boards.
- AC precharge circuit board and torque accuracy module (if present) fiber-optic cables from the ACP0 and ACP1 / TAM port, respectively.
- Each line side inverter fiber-optic cable from the Lnport.
- Each motor side converter fiber-optic cable from the Mnport.
Port NameDescriptionACP0Fiber transceiver port for the fiber-optic connection from ACP on the first AC precharge control board.ACP1 / TAMFiber transceiver port for the fiber-optic connection from ACP on the second AC precharge control board (frames 13…15 only) or the fiber-optic connection from TAM on the torque accuracy module. Frame 13…15PowerFlex®755TR drives and 755TM bus supplies cannot use a torque accuracy module (TAM).L0…L9Fiber transceiver ports for the fiber-optic connections from CNTL on the power layer interface board in power modules that are used as line side converters.M0…M9Fiber transceiver ports for the fiber-optic connections from CNTL on the power layer interface board in power modules that are used as motor side inverters. - Follow the minimum bend radius requirement and carefully coil the fiber-optic cable and secure in a protected location.
- If an option module is installed, complete these steps:
- Disconnect the plug-in terminal blocks.
- Loosen the two captive thumbscrews that secure the option module to the control pod chassis and remove the option module. Final torque for reassembly is 0.45 N•m (4.0 lb•in).
- Record any settings that are made on these main control board selectors or jumpers (B):
- Control selector
- EmbeddedEtherNet/IP™address selectors
- Safety enable jumper
- Hardware enable jumper
- Disconnect any Ethernet cables from the Ethernet ports (C) on the bottom of the main control board.
- Disconnect the plug-in terminal block TB1 (D) on the bottom of the main control board.
- If present, disconnect theDPI™cable from the mini-DIN Port 2 connector (E) on the control pod chassis.
- Disconnect connector P14 from connector J14 on the fiber-optic interface board.
- If installed, disconnect the customer supplied 24V supply power wire connector P13 from connector J13 on the fiber-optic interface board.
- Loosen the four M4 x 8 mm Torx screws that secure the pod chassis to the back panel.
- Slide the pod up, so that the keyholes on the pod clear the mounting screws, and remove the control pod.
- TIP: Control pod mounting panel shown in example.
- Install the control pod in the reverse order of removal.
- Make any necessary changes to the settings on these main control board selectors or jumpers:
- Control selector
- EmbeddedEtherNet/IP™address selectors
- Safety enable jumper
- Hardware enable jumper
- For each fiber transceiver board, open the transceiver latch and pull the transceiver out of the connector on the board.
- TIP: If the latch is obstructed and you cannot use your fingers to open it, use a small, screwdriver or other long, narrow tool to open the latch.
- Without bending the cable to a radius less than 50 mm (2 in.), fully insert the fiber-optic cable into the transceiver.
- Insert the transceiver and fiber-optic cable into the connector on the board, until you hear an audible ‘click.’
Provide Feedback