View the Synchronization Log

On the Synchronization tab of the RMCT, you can view a log of synchronization events. If qualification of the redundant chassis pair fails, use the synchronization log to help identify and resolve the cause.
Synchronization Log
Synchronization Log
Synchronization Log Parameters
Parameter
Description
Event No.
A unique, sequential number to identify the event.
Time Stamp
The date and time that the event was logged.
Basic Info
A basic description of the synchronization event. If qualification did not succeed or a fault is indicated, refer to the Extended Info columns to diagnose the cause.
Extended Info 1
Extended Info 2
Additional information that is related to the basic description of the event. Extended Info 2 information is not available for every event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal