Install the RMCT
FactoryTalk® Linx
RMCT must be installed on the same computer as the FactoryTalk® Linx
Network Browser. You can access FactoryTalk® Linx
RMCT only from the FactoryTalk® Linx
Network Browser.To install the RMCT, follow these steps.
- Browse to the RMCT directory on your computer.
- Double-click setup.exe.
- On the RMCT Setup dialog box, select Next.
- When the installation is complete, select Finish.
Provide Feedback