Load a Project from the Memory Card
If you must load a project from the memory card, you must first disqualify your redundancy system. You then load the project from the memory card to the primary controller and resynchronize the redundant chassis once the load process is complete.
For details about loading a project from the nonvolatile memory card, see the Logix 5000 Controllers Nonvolatile Memory Card Programming Manual, publication 1756-PM017.
Provide Feedback