Security Considerations

To help maintain a secure system, follow these guidelines:
  • Limit physical access to authorized personnel.
  • Implement physical barriers, such as locked cabinets.
  • Only purchase products from official suppliers.
  • Only download firmware and software from the Rockwell Automation official download portal at rok.auto/pcdc.
To secure networks and communication and data, follow these guidelines:
  • Implement network technologies that filter, block, and control access to help secure networks.
  • Configure authorization policies to define conditions for remote access.
  • Select control products that offer security options.
To align your system with IEC 62443-4-2 security technical requirements, see Develop Secure High Availability Systems.
For more security-related information, see the following publications.
Resource
Description
System Security Design Guidelines Reference Manual, publication SECURE-RM001
Provides guidance on how to conduct vulnerability assessments, implement Rockwell Automation products in a secure system, harden the control system, manage user access, and dispose of equipment.
Configure System Security Features User Manual, publication SECURE-UM001
Describes how to configure and use Rockwell Automation products to improve the security of your industrial automation system.
CIP Security with Rockwell Automation Products Application Technique, publication SECURE-AT001
Describes how to plan and implement a Rockwell Automation system that supports the
CIP Security
protocol.
FactoryTalk Security Application Technique, publication SECURE-AT002
Describes how to How to use
FactoryTalk® Security
to implement authentication and authorization in your industrial automation system. Describes how to enforce product-specific security for
Studio 5000 Logix Designer®
,
FactoryTalk® View
, and
FactoryTalk® AssetCentre
.
Converged Plantwide Ethernet (CPwE) Design and Implementation Guide, publication ENET-TD001
Provides guidelines for how to design, implement, and manage industrial Ethernet networks.

Redundancy Module MicroSD Card Security

1756-RM3 redundancy modules have a
microSD
card for the primary purpose of storing Tech Support logs that Rockwell Automation can use to investigate the cause of a fault.
The
microSD
card is secured in the following ways:
  • Major fault data for the 1756-RM3 is stored on the
    microSD
    card in the Rockwell Automation folder. All sensitive data in this location is encrypted and only Rockwell Automation can decode the encrypted data.
  • Data is saved to the
    microSD
    card in only one direction: from the internal memory of the redundancy module to the
    microSD
    card.
  • Data stored on the
    microSD
    card cannot be read by the redundancy module firmware.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal