Supported Features

The following features are supported in high availability systems:
  • CIP Security
  • CIP Sync
  • Produced/consumed standard tags
  • Produced unicast connections
  • Produce/consumed multicast connections
  • PlantPAx®
    for process controllers
  • FactoryTalk®
    applications for communication modules
  • SequenceManager
    for process controllers
  • PhaseManager
  • Firmware Supervisor
  • EtherNet/IP
    socket interface
  • Parallel Redundancy Protocol (PRP)
  • Device Level Ring (DLR)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal