Configure Front Port Crossload Mode
Front Port Crossload mode is a communication mode that improves scan time performance by crossloading task data through the front Ethernet ports on the controller. Scan time decreases by 2x when data is crossloaded through the front ports compared to the backplane. For details, see Estimate Crossload Time per Sync Point.
Front Port Crossload Enabled Checkbox

This mode is disabled by default in the Logix Designer application.
IMPORTANT:
When redundancy is enabled, note the following:
- The controller Ethernet ports are reserved exclusively for crossloading data.
- The ports do not appear in the I/O Configuration tree in the Logix Designer application.
- Attempts to use the Ethernet connections for any other purpose than crossloading data are rejected.
Media Redundancy
The two Ethernet ports on each redundant controller provide optional media redundancy to
avoid a single point of failure. You are not required to use both front ports. If one port
is used for crossloading data, the other port is reserved exclusively for crossloading data
and does not support other communication functions.
Ethernet Port IP Addresses
By default, this mode is enabled with fixed IP addresses assigned to the ports. The status display on the front of the controller does not show the assigned IP addresses of the front ports. To indicate this port configuration, the controller displays the following message on its status display:
Link x crossload-redundan-en
Requirements and Restrictions
Front Port Crossload mode has the following requirements and restrictions:
- Use only a point-to-point connection between the ports. No media converters or switches are allowed between the ports.IMPORTANT: A point-to-point connection limits the allowable physical distance between the redundant chassis to the maximum supported length of the Ethernet cable, which is typically 100 meters.
- Only crossloaded data is permitted through the ports and general traffic is prohibited. Crossloaded data includes HMI, MSG instructions, going online, webpage access, I/O, and produce/consume data.
- Changes to the Front Port Crossload mode (enable or disable) take effect only when you download the project to the controller.For more information, see Download the Project.
- After a project is downloaded to the secondary controller during the Redundancy System Update (RSU) process, changes to the Front Port Crossload mode (enable or disable) cause the RSU process to cancel.For more information, see Download the Project the Secondary Controller.
- When Front Port Crossload mode is enabled, you cannot browse to the secondary controller through the front ports viaFactoryTalk® Linx.
Diagnostics
You can use logic to access diagnostics for the front Ethernet ports on the controller. See
Obtain Controller Front Port Status.
Provide Feedback