Connect to Safety I/O
Before you use safety I/O, do the following:
- Read, understand, and follow all safety information in the product documentation for those products.As the range of products using theCIP Safety™protocol continues to expand, there are variations to the typical safety I/O configuration steps. Product specific procedures and requirements can include the following:
- Reset of ownership
- Setting the safety network number
- Configuration signature generation
- Requested packet interval (RPI) limits
- Device-specific configuration settings
For more information, see the user manual for your I/O device. - Commission all devices with a node or IP address and communication rate before their installation on a safety network.
Network Address Translation
Network Address Translation (NAT) translates one IP address to another IP address via a NAT-configured router or switch. The router or switch translates the source and destination addresses within data packets as traffic passes between subnets. This service is useful if you must reuse IP addresses throughout a network. For example, NAT makes it possible for devices to be segmented into multiple identical private subnets while maintaining unique identities on the public subnet, such as for multiple identical machines or lines.
This section only applies to safety users where the controller and the devices it talks to are on separate sides of the NAT-configured router or switch.
With
CIP Safety™
, the IP address of the device is part of the unique node reference that is part of the protocol. The device compares the IP address portion of the unique node reference in CIP Safety™
packets to its own IP address, and rejects any packets where they do not match. The IP address in the unique node reference must be the NAT'ed IP address. The controller uses the translated address, but the CIP Safety™
protocol requires the actual address of the device. If you use NAT to communicate with a
CIP Safety™
device, use the Advanced Ethernet Settings when you configure the IP address and enable 'Module and controller communicate through Network Address Translation (NAT) devices.'.Safe State
Safety I/O has most of the attributes of standard I/O except it features mechanisms that are certified to SIL 2 or SIL 3 for data integrity. A safety input is a combination of produced and consumed safety tags, mapped safety inputs, and inputs from safety modules.
Before you use safety I/O, do the following:
- Read, understand, and follow all safety information in the product documentation for those products.
- Commission all devices with a node or IP address and communication rate before their installation on a safety network.
Safety I/O devices, like sensors and actuators, can be connected to safety input and output modules. The controller monitors and controls the devices. For safety data, I/O communication is performed through safety connections by using the
CIP Safety™
protocol. Safety logic is processed in the controller.
ATTENTION:
- The safe state of the outputs is defined as the off state.
- The safe state of the module and its data is defined as the off state.
- Use safety I/O modules only in applications where the off state is the safe state.
Safety I/O treats the following as the safe state:
- Safety outputs: OFF
- Safety input data to controller: OFF
Safe State
IMPORTANT:
If you inhibit a safety module from transitioning to a safe state when a fault occurs because an I/O connection is lost, you accept responsibility for any consequences that result from your decision to inhibit. We recommend that you use other means to maintain the safe state if you inhibit the safety module from transitioning to a safe state.
Configuration Signature and Ownership
One controller owns each safety I/O device in a non-redundant safety system. Multiple controllers and multiple safety I/O devices can be used in chassis or on networks. When a controller owns an I/O device, it stores the configuration data that you define for that device. This configuration controls how the devices operate in the system.
From a control standpoint, one controller controls safety output devices. One controller also owns each safety input device. However, safety input data can be shared (consumed) by multiple controllers.
Configuration | Description |
|---|---|
Configuration Signature | Each safety device has a unique configuration signature that defines the module configuration. The configuration signature includes the following:
The configuration signature is used to verify a module’s configuration. The signature can only be considered “verified” (and configuration locked) after user testing. |
Configuration Ownership | The connection between the owner-controller and the safety module is based on the following:
If any differences are detected, the connection between the owner-controller and the safety module is lost, the yellow yield icon appears in the controller project tree. |
When a controller owns the I/O module configuration, other controllers can listen to the input module. In this case, the module configuration signature in the Logix Designer project for any listening controller must match the one in the owner-controller project.
- If the safety module is configured for inputs only, you can copy and paste the configuration signature from one project to the other.
- If the safety module has safety outputs, for example, the configuration signature parameter is disabled.
Safety Rating Considerations
Input and output configurations can affect safety ratings.
Configuration Type | Description |
|---|---|
Input | Some safety input modules have safety inputs that can be configured as single or dual (Equivalent or Complement) point operation types. The selected type configures the safety module to view the inputs individually or as a pair:
The method of monitoring discrepancy has no impact on the safety rating. The main effect is the availability of diagnostic information:
|
Output | For output modules, sourcing safety outputs can be configured as point operation type single or dual. The selected type configures the safety module to treat the outputs individually or as a pair:
Bipolar outputs have no configuration for point operation type and must operate as a sinking sourcing pair. The point operation type affects the PFH safety rating of the module. The PFH is the average frequency of a dangerous failure per hour. |
Provide Feedback