Module Tag Definitions
Module tags are created when you add a module to the Studio 5000 Logix Designer
application project. The set of module tags associated with a module depends on the
module type and Device Definition choices made during module configuration. The tables
contained in this section list all of the tags available with a module. Not all tags in
the list are used when that module type is added to a project. Tag use varies by module
configuration.
Provide Feedback