Create Message Type User Tags
Create MESSAGE type user tags for requests and associated response user tags for each of
the new user-defined diagnostic assembly types.

From the
Controller Organizer pane, expand Tasks → MainTask → MainProgram:
- Create MESSAGE type user tags for each request.
- Create associated response user tags for each new user-defined diagnostic assembly type.
- Add the user tags to your ladder program.

- Expand the message tag to open the message configuration dialog.
- On the Configuration tab, select:
- On the Communication tab, select the path to the module that you wish to send the messages to.
- Download the project and set to Run mode.You can monitor the user-defined tag values from the Program Parameters and Local Tags window, under the MainProgram task in the Controller Organizer pane.
Provide Feedback