Module Tag Definitions
Module tags are created when you add a module to the Studio 5000 Logix Designer
application project.
The set of module tags associated with a module depends on the module type and Module
Definition choices made during module configuration.
The tables contained in this section list all of the tags available with a module. Not
all tags in the list are used when that module type is added to a project. Tag use
varies by module configuration.
Provide Feedback