Export FactoryTalk Smart Object configuration values
Export
FactoryTalk Smart Object
configuration values to a .csv
file to update values quickly. Use the CSV file to filter and modify FactoryTalk Smart Object
configuration values. After modifying the
FactoryTalk Smart Object
configuration values in the .csv
file, import the FactoryTalk Smart Object
configuration values to Studio 5000 Smart Object Configurator
.To export
FactoryTalk Smart Object
configuration values- SelectExport
. - SelectFull configuration.
- SelectExport.
- Select a location and type a file name.
- SelectSave.A.csvfile is created.
- Modify the spreadsheet. Columns that are read-only contain (r) in the column heading.TIP: Files exported from the Smart Object Configurator application are unencrypted plain text that may contain sensitive information. You must ensure that the data is always secured, encrypted, and proper permissions are set to those files to prevent unauthorized modification. It is recommended that you store the files on local machine.
Provide Feedback