Customizing the Ladder Common Logic Toolbar

To customize the Ladder Common Logic toolbar:
  1. Add and remove buttons to configure your toolbar.
    Select the
    arrow
    buttons to add and remove toolbar buttons.
  2. Select
    OK
    to accept your toolbar configuration.
  3. Select
    Close
    to close the Toolbars dialog box.
To access the Customize Toolbar - Ladder Common Logic dialog box:
  1. From the
    View
    menu, choose
    Toolbars
    .
    The
    Toolbars
    dialog box appears.
  2. Select the
    Ladder Common Logic
    toolbar from the list.
  3. Select
    Customize.
    The
    Customize Toolbar - Ladder Common Logic
    dialog box appears.
    TIP: If FactoryTalk Security is enabled, this dialog may be disabled, depending on the levels of access that have been defined. For details about FactoryTalk Security, see FactoryTalk Help:
    Start > Programs > Rockwell Software> FactoryTalk Help
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal