Go Online Using Recent Communications Path dialog
Use this dialog to go online using a recent communications path. It is similar to the
Select Recent Communications Path
dialog, except that instead of simply using it to
choose a path, the Logix Designer
application also attempts to go
online using that path.Parameters
Controller
Select the controller with which to go online.
Path
Select the communications path with which to go online.
Go Online
Select to go online using the selected recent communications path.
Provide Feedback