Driver and Path Configuration dialog settings

Use the
Logix Designer
application
Driver and Path Configuration
dialog to manually enter a communications driver path for a driver that is already created. See Enter a communications driver and path manually.
TIP:
  • Create Ethernet drivers in the
    Logix Designer
    application
    Network Browser
    dialog or
    FactoryTalk Linx
    Network Browser dialog.
  • Create ControlNet and DH+ drivers in the
    FactoryTalk Administration Console
    for
    FactoryTalk Linx
    .
Following are the
Driver and Path Configuration
dialog settings:
Setting
Description
Driver
Used to select from the list of running drivers in the
FactoryTalk Linx
communication software.
Path
Enter the CIP path to a controller that
Logix Designer
uses when executing a
Go Online
,
Upload
, or
Download
command. The path also writes to any project.
TIP: For
ControlNet
and
DH+
, construct the path starting from the communications module in the local chassis. Separate the number or addresses entered in each step with a comma. All numbers are decimal, by default. Enter any number other than an Ethernet/IP address in another base by using an IEC-1131 prefix ("8#" for octal, "16#" for hexadecimal). Ethernet/IP addresses are always dot-separated decimal numbers.
Recent
Navigates to the
Select Recent Communications Path
dialog, and select a recent saved path as the current communications path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal