Export dialog box
Use the
Export
dialog box to specify the file that will contain the exported content.
TIP:
To open the Export dialog box, right-click a component in the Controller Organizer and select
Export
.This table describes the dialog box parameters.
Parameter | Description |
|---|---|
Save in | The folder where the export is saved. |
File name | The file name for the export. To clearly identify the type of file being exported, the component type is appended to the file name as follows:
|
Save as type | The type of file that is to be exported. The default is Logix Designer XML File (*.L5X) and cannot be changed. |
File description | A description for the export (optional). The description is saved with the exported file and appears in a tooltip when a cursor hovers over the file. |
Include all referenced Add-On Instructions and User-defined Data Types | When selected, all referenced Add-On Instructions and User-defined Data Types are included with the exported content. When unselected, only the Add-On Instruction or User-defined Data Type is exported, and any Add-On Instruction or User-defined Data Type nested within the exported component are excluded. This setting is selected by default, and the setting is retained. This check box appears only for Add-On Instructions and User-defined Data Type exports. All other export types act as though this field was checked. |
Export | Exports the selected component. If you are online, you are prompted to upload tag values. When you select Yes , the Logix Designer application uploads all tag values in the current ACD file from the controller and creates the export file using these new tag values. When you select No , the export file is created using the tag values currently stored in the ACD file (which may be different from the tag values displayed while online). |
Encode protected content | Exports protected content in encoded format. Routines and add-on instructions can be exported in an encoded format when they are protected with FactoryTalk Security , or Source Protection or both.This setting can be changed only when the Always Encode Protected Content on Export check box in the Workstation Options dialog box is cleared.
TIP:
When exporting a component that does not
support being exported encoded, this checkbox still controls the encoded export of
any referenced components, such as routines or add-on instructions, that can be
exported encoded.
TIP:
Protection permissions (for example,
permissions configured in
FactoryTalk Security or Source Protection) can
override this selection. When this checkbox is cleared, the component is still
exported encoded even if you do not have permission to export unencoded. |
Include all child modules | When selected, all modules configured under the module are included in the export file. When unselected, only the selected module is exported. This setting is selected by default. This check box appears only for module exports. |
Provide Feedback