Unable to import programs
If a conflict occurs during the import, you will see the following message:
Unable to import programs. The existing programs will be used.
When performing an import in Run mode, pay particular attention to the configuration of the import.
- Programs cannot overwrite Equipment Phases and vice versa.
- Routines cannot overwrite routines of a different type (that is, a Ladder Diagram cannot overwrite a Function Block Diagram).
- Do not overwrite a program if the assigned routines are different. The existing program is used.
- Do not overwrite a tag online that already exists in the project and has a different data type. The existing program is used.
If collisions occur, the operation for the component is forced to
Use Existing
. It is important to review how the other components are configured. It is also important to understand the impact of importing the other components without importing the discarded component.Provide Feedback