Write a fault routine
A fault routine normally contains logic to identify the program fault. Some fault routines also contain logic to clear the fault. If a fault is cleared, the ladder program continues executing at the instruction immediately after the instruction that caused the program fault, and the controller does not enter fault mode. If a fault routine does not clear the fault, the Controller Fault Handler program is invoked.
Provide Feedback