Print dialog box settings
Use the
Print
dialog box to specify a printer and modify its properties, as well as customize your print job.Parameter | Description |
Name | Printers that are set up on your computer. |
Status | Status information for the selected printer. |
Type | General information about the selected printer. |
Where | Port or network print queue information for this printer. |
Comment | General information about the selected printer. |
Properties | Select this button to set up options for this printer. Available options depend on the features of the specified printer. |
Print Range | Choose whether you wish to print all, a selection of, or a range of items. These options are currently only enabled for printing from the Tag Editor/Data Monitor, and each of the language editors. Note that this selection is only applicable when you have selected something from the active window. |
Number of Copies | Enter the number of copies you wish to print. |
Print Options | Select this button to go to the Print Options dialog box. |
OK | Select this button to accept your edits, start the print job, and close the Print dialog box. |
Cancel | Select this button to cancel your edits and close the Print dialog box. |
Provide Feedback